Skip to content

Medical

Motion you can put next to a patient.

Smooth, near-silent, micron-repeatable motion for surgical robots, imaging equipment, and medical devices, in sizes from full-scale imaging gantries down to 2mm miniature guideways.

A close-up of an automated laboratory pipetting machine dispensing liquid into numerous small test tubes arranged in rows on a tray.

2mm

Smallest miniature guideway — sized for bioprinters and dispensing

ISO 9001 + 14001

First motion control manufacturer in the world certified to both

35+

Years engineering precision motion

Applications

Built into the equipment that cares for patients.

From the gantry that circles a patient to the axis that places a single droplet, HIWIN components are already at work across the device landscape.

  • Imaging systems

    Ballscrews and guideways move CT and MRI patient tables smoothly enough for artifact-free scans.

  • Medical beds

    Linear guideways carry the sliding, reclining, and pivoting motion patients feel directly.

  • Surgical robots

    Micron-level repeatability on every axis, with the rigidity a moving instrument demands.

  • Rotary lab equipment

    Torque motors deliver precise angular positioning for centrifuges and rotating stages.

  • 3D bioprinters

    Miniature guideways and ballscrews position print heads at cell-culture scale.

  • Liquid dispensing

    Guideways down to 2mm place droplets with the repeatability diagnostics depend on.

A man in a white shirt explains products to two smiling attendees at a trade show booth, surrounded by displays and other people in a brightly lit exhibition hall.

Why HIWIN

Precision is a patient-safety spec.

Your equipment operates where other machines never could: sterile environments, beside patients, mid-procedure. A hospital bed that hesitates, an imaging gantry that vibrates, a surgical axis that drifts: in medical devices, mechanical disruption isn’t a maintenance ticket, it’s a patient risk. And you’re expected to qualify components faster than ever while proving they’ll run reliably for the life of the device.

HIWIN builds motion components for exactly these constraints: smooth, near-silent travel with near-zero friction, in a range of sizes that spans full imaging systems down to 2mm miniature guideways for liquid dispensing and 3D bioprinting. Medical OEMs and suppliers get the precision and safe operation that patient contact demands, from a manufacturer whose quality system is certified, not just claimed.

Products

A full range of system components for precision motion control.

Browse all products →
  • A linear guide rail with a metal carriage block mounted on a steel track, used for precise linear motion in machinery. The block has green and red end caps and mounting holes.

    Beds · Imaging · Bioprinting

    Linear Guideways

    Smooth, near-zero-friction travel for hospital bed adjustment and patient positioning on MRI and CT scanner tables, with miniature sizes down to 2mm for liquid dispensing and 3D bioprinting.

    Browse linear guideways →
  • A silver ball screw with a flanged nut, shown on a white background. The mechanism features helical grooves on both the screw shaft and inside the nut.

    Imaging · Examination tables

    Ball Screws

    The precision, repeatability, and accuracy to move heavy imaging equipment seamlessly enough for high-quality scans. Miniature ballscrews serve dispensing machinery and bioprinters.

    Browse ballscrews →
  • 3D-rendered image of a linear motion guide with an attached cable, featuring a black and silver design with colored accents, labeled HIWIN on one end, shown on a plain white background.

    Dynamic positioning

    Linear Motor Stages

    Dynamic, precise positioning for smooth motion in medical equipment, often paired with supplemental drives and controllers that further improve movement capabilities.

    Browse stages →
  • A close-up of a cylindrical metal electric motor with grooved outer layers, a hollow center, and two wires—one black and one orange—extending from the side.

    Centrifuges · Rotary tables

    Torque Motors

    Rotary motion with precise angular positioning and seamless movement, frequently found in rotating laboratory equipment such as centrifuges.

    Browse torque motors →

Researching a design? Download catalogs and application notes →

Application story

Qualifying 2mm guideways for a next-generation surgical platform.

A surgical-robotics manufacturer needed miniature linear motion for an instrument-positioning module: small enough for a 2mm envelope, quiet enough for the OR, and supplied with the material and process documentation their design-history file required. Working with HIWIN application engineering, the team selected miniature guideways with low-particulate lubrication, validated repeatability on HIWIN test data, and moved from first samples to design freeze in a single development cycle.

“We needed an axis we could hold to microns, run near-silent beside an anesthetized patient, and document to our auditor’s satisfaction. HIWIN’s application engineers were in the design reviews with us.”
— Principal mechanical engineer, surgical-robotics OEM
Two people in white shirts are holding and examining a metallic mechanical component with multiple holes and grooves, likely discussing its design or function.

2mm

Guideway envelope qualified

±3µm

Repeatability validated on the instrument axis

1 cycle

From first samples to design freeze

FAQ

Medical motion control, answered.

Still weighing a design decision? Ask an application engineer →

Can HIWIN components be used in cleanrooms and sterile environments?

Yes. Guideways and ballscrews are available with low-particulate greases, corrosion-resistant materials, and sealing options suited to cleanroom and medical-adjacent environments. Our application engineers will match the lubrication and sealing package to your cleanliness classification.

What is the smallest linear guideway HIWIN offers for medical devices?

Miniature linear guideways start at a 2mm rail width, small enough for liquid dispensing heads, 3D bioprinters, and instrument-positioning modules inside surgical systems, while keeping the smooth, low-friction travel of full-size guideways.

How quiet are HIWIN guideways for patient-adjacent equipment?

HIWIN linear guideways are engineered for smooth, near-silent travel with near-zero friction. That makes them a common choice for motion patients experience directly: hospital bed adjustment, imaging tables, and surgical axes that operate beside an awake or anesthetized patient.

What quality certifications does HIWIN hold?

HIWIN was the first motion control manufacturer in the world certified to both ISO 9001 and ISO 14001. Component-level documentation is available to support your design-history file and supplier qualification process.

Does HIWIN provide engineering support during device qualification?

Yes. HIWIN application engineers support medical OEMs from concept through qualification: sizing and selection, CAD models, sample components for validation builds, and test data to support your verification documentation.

Which medical applications already use HIWIN components?

HIWIN motion components are at work in CT scanners, MRI machines, hospital beds, examination tables, surgical robots, centrifuges, 3D bioprinters, and liquid dispensing machinery, spanning full-scale imaging gantries down to 2mm miniature axes.

A persons hands install a metal bearing onto a long, cylindrical metal rod in a workshop or industrial setting. Shelves and equipment appear blurred in the background.

Medical

Designing a medical device? Talk it through with an application engineer.